Part Number: SN65DSI83-Q1
Other Parts Discussed in Thread: DSI-TUNER
Tool/software:
We are working in the SN65DSI83-Q1 and integrated with the LTK101FTNCT54 display in the SC668s som board the issue is the DISPLAY not working and it doesn;t show the Test pattern also.
Below the schematics added

Logs :
trinket:/ # i2cdump -f -y 2 0x2c
Debugged the issue in the below method:
1. Checked the 0xe5 registers it showing 0x3d which means there is error.
2. After enabled the CONVERT_DEBUG in driver file
3. Writes 0xFF in register 0xe5
4. After its read 0x01 still the error shows.
Note:
sometimes the 0x0a shows if the Android screen wakes it shows the 0x83 and the android screen goes sleep then t shows 0x03
Can you please help us to resolve the issue
Regards,SanthanaKumarS