Part Number: TCAN1043-Q1
Tool/software:
Hello,
I am using TCAN1043-Q1 CAN transceiver, if there are 10 nodes on CAN bus with 120-ohm termination resistor at each node, then the equivalent resistance between CAN H and CAN L will be only 12 ohms.
In this case, this is near to short circuit condition or if more nodes (100 as per datasheet) are connected max current will flow through the termination resistor?
So, the effective communication happens in this case ?