Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0104: Pull-up Supply & Resistor

Part Number: TXB0104
Other Parts Discussed in Thread: TXU0304, TXU0104, TXU0204

Tool/software:

Hi Team,

Customer feedback that the input voltage of B ports will influence by the outside pull-up resistor, under 3.3V pull-up supply:

  • With 10kohm resistor, the voltage of B ports is 1V
  • With 100kohm resistor, the voltage is ~0V
  • With 2kohm resistor, the voltage is right 3.3V

Based on #1, seems the internal impedance is ~4.348kohm, but it cannot meet the #3, could you please help check it and explain it to customer? Thanks.

BRs,

Francis