This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UH988-Q1: resolution of 2560*1440

Part Number: DS90UH988-Q1


Tool/software:

Hi ti team,

Is the output interface of the DS90UH988 chip compatible with the LVDS standard and support a resolution of 2560*1440?

  • Hi,

    Is the output interface of the DS90UH988 chip compatible with the LVDS standar

    DS90UH988 is compatible with OLDI(Open LVDS Display Interface) standard built on LVDS physical.

    support a resolution of 2560*1440?

    Your desired refresh rate, blanking pixels and pixel resolution are needed to determine if DS90UH988 can provide a suitable PCLK and data-rate for your 2560x1440 display needs. 

    For example, assuming the following requirements:

    Total pixels = (active pixels) x 1.15 =  i.e blanking is 15% of active pixels

    refresh rate = 60Hz

    pixel resolution = 24-bit

    PCLK = (2560x1440) x 1.15 x 60 = 254.36MHz PCLK

    data-rate = 254.36MHz x 24 = 6.1 Gbps FPD-LINK IV line rate

    In this example scenario, the DS90UH988 would be suitable for the 2560x1440p display using Dual Link OLDI output. 

    Please provide more details on your application such as total pixels, refresh rate, number of displays for further guidance.

    Thanks,

    Ragav Subramanian