Part Number: DS110DF410
Tool/software:
Hi team,
I have some questions regarding the pin settings.
1) When using the DS110DF410 with the CDR bypassed, is it necessary to input a reference clock? In that case, can the REFCLK_IN/OUT pins be left open?
2) If only channel 0 is used, can the RXP/N, TXP/N, LPF_CP, and LPF_REF pins for channels 1, 2, and 3 be left open?
3) The pin description for LPF_CP and LPF_REF in the datasheet states, "Place a 22 nF ± 10% Capacitor between LPF_CP_0 and LPF_REF_0." On the other hand, the EVK allows these two pins to be shorted. In what situations should they be shorted?
Sincerely,
Naoki Yoneyama