Part Number: TL16C752D
Other Parts Discussed in Thread: TL16C752C, , TL16C754C
Tool/software:
Hi team,
Please tell us some of them.
I would like to receive an answer for each item.
- Differences between TL16C752D and TL16C752C
- Should the trigger level for the transmit FIFO be specified by the number of empty buffer sizes?
Or should it be specified by the number of data to be sent? - Does an interrupt occur when the number of data to be sent or the number of empty buffer sizes reaches (equals) the number of trigger levels?
Does an interrupt occur when the trigger level is exceeded? - If a transmission is performed with only the number of transmit data in the transmit FIFO that does not exceed the trigger level, interrupts that exceed the transmit trigger level will not be generated.
Is it correct to assume that a transmit empty interrupt is generated for a transmission that does not exceed the trigger level? - After an interrupt that crosses the transmit FIFO trigger level is received and the interrupt is released by reading the ISR register, will the transmit empty interrupt be received?
- Is it correct to assume that when Auto RS485 mode is enabled and 485LG is OFF, the interrupt by the FIFO trigger level will not be triggered?
- When Auto RS485 mode is enabled, if 485LG is ON, interrupts are triggered by the FIFO trigger level, but not the transmit complete (TSR empty) interrupt, but the empty (THR empty) interrupt, is this correct?
- Although not made by TI, the following Errata was found in a serial controller from another company.
(Errata contents) When a transmit interrupt is received at the timing when the ISR register is read by the receive interrupt, the transmit interrupt is canceled by reading the ISR register and the transmit interrupt is missed.
Is it safe to assume that there is no such Errata?
Best Regards,
Ryu.