This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9406: TCA9406 VOL Issue

Part Number: TCA9406
Other Parts Discussed in Thread: TCA9517A, TCA9617B, TCA9517

Tool/software:

hi

i'm using TCA9406 and i see at the output that sometimes the "0" is not going below 0.54V , it causes to missing bits (probably) 

the PU resistor we use is the internal TCA9406 resistor (10KOhm)

i added picture of scope : yellow trace is CLK  , Green trace is data where sometimes the "0" is not going below 0.54V.

will appreciate any ideas