This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS100BR210: Unused Channel B Pin Configuration

Part Number: DS100BR210

Tool/software:

Hi All,

I'm designing a new board using the DS100BR210.

I only need to use Channel A. In this case, what should be the state of the Channel B control pins (pins 1, 2, 5) and video pins (I believe pins 11 and 12 should be set to '0', and pins 19 and 20 should be left floating)?

Thanks

  • Hi Yoav,

    The control pins can be left floating.

    You are correct that pins 11 and 12 should be set to '0'. They should be AC terminated to GND with AC capacitors and a resistor.

    and pins 19 and 20 should be left floating.

    Best regards,

    Nick