Part Number: SN65DSI83
Tool/software:
Hi team,
On my design, The processor's MIPI DSI signals are connected to an SN65DSI83 bridge.
The MIPI DSI clock is configured with following parameters:
- Freq :156MHz
- Spread spectrum :+/-2%
=> The DSI clock frequency varies from 152.88MHz and 159.12MHz.
I don't know which value should be used to configure the CHA_DSI_CLK_RANGE register (0x12) :
0x1F : 155MHz ≤ DSI clock frequency < 160MHz
0x20: 160MHz ≤ DSI clock frequency < 165MHz
Which value should be use to configure the CHA_DSI_CLK_RANGE register (0x12)?
Best Regards
Sylvain