Part Number: TCAN1145-Q1
Other Parts Discussed in Thread: TCAN4550-Q1
Tool/software:
Hi expert,
Does the TCAN1145 have a mechanism to transmit time delay compensation (TDC) and a secondary sample point? Currently the measured CANFD data segment sampling point is lower than the setting and R&D wants to know if this is related to the configuration of TCAN1145 and if this can be resolved by TCAN1145? Thanks.
- Issue background: The measured CANFD segment sampling point is always lower than the software configured sample point value, which cannot meet customer request. The data segment sampling point requirement for the CANFD network is to meet the [78%, 82%] interval. The actual sample point will be lower than 78%.
Best Regards,
Ryker