Part Number: DS90UB933-Q1
Tool/software:
Hi ti team,
Does the output of DS90UB944 support a screen with a resolution of 3036 (RGB) * 1708?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB933-Q1
Tool/software:
Hi ti team,
Does the output of DS90UB944 support a screen with a resolution of 3036 (RGB) * 1708?
Hi switch,
Please provide more details on your configuration and video settings for better support.
Assuming the following video settings:
The calculation would be as follows to determine bandwidth:
Pactive = 3036 * 1708
Pblanking = 0.15 * Ptotal
Ptotal = Pactive + Pblanking
PCLK = Ptotal * 60Hz = 357.8 MHz
FPD datarate = PCLK * 30-bit color = 10.73Gbps
In this scenario, the FPD data-rate falls within the bandwidth (13.5Gbps FPD-Link III with dual port config); therefore, the DS90UB944 would support the resolution.
Please ensure you are using 5.4Gbps 4-lane DP at minimum to support given resolution. Refer to calculation below:

Thanks,
Ragav Subramanian