Part Number: SN65HVD3088E
Tool/software:
Dear
About the internal capacitance between A and B (Bus input/output) of the SN65HVD3088 RS-485 transceiver
Used as an RS-485 transceiver in the CCLink circuit
The stray capacitance of outputs A and B is large, which is causing problems.
I think the problem is that the internal capacitance between A and B of the RS-485 transceiver is large.
question
What is the internal capacitance between A and B of the SN65HVD3088E?