Part Number: TUSB1104
Tool/software:
Hello support team,
My customer decides to use our redriver TUSB1104 at USB-C application.
And there is the issue that the device is only be able to be linked at USB3.2 gen2 x1, which means only one side of SSTX/RX is working.
I firstly eliminate the issue with layout mismatch issue, the redriver is put between at the middle of the USB-C connector and CPU (RPL-S platform).
Here's my register setting at USB-C port, may you help to clarify if this is the correct one?
Power on / Reset:
Set 0x24 and 0x25 register to 11h (Enable the bit 4 for USB3.2x2)
Set the 0xA register to 11h
Detach device:
Set the 0xA register to 11h
Upside-up orientation connection:
Set the 0xA register to 11h
Upside-down orientation connection:
Set the 0xA register to 15h (Flip bit is asserted)
I didn't change anything about the EQ part due to the default setting for adaptive EQ.
Did I miss anything at TUSB1104?
Thanks for the suggestion.
Best regards,
Dave