Part Number: SN65DSI86
Tool/software:
Hello:
1. When designing with SN65DSI86ZQER, AUXP and AUXN are reversed. Can I switch between AUXP and AUXN internally in the TI chip?

2. What are the impacts of reversing? Does it affect the normal display of the screen? The current EDP eye diagram test is passed.
3. There are 100K up and down buttons on AUX P/N, and if PN is reversed, the up and down buttons will also be reversed; Does it affect the normal operation of the chip?
4. The up and down buttons of this aux are used not only for communication, but also to inform the screen that the source side is ready; Does this reversal have an impact on the mechanism?
Thanks!!!