Part Number: SN75LVDS82
Tool/software:
Hello, I need your help.
I have to convert an LVDS-to-RGB signal, and the LVDS signals have a +1V8 level.
Is the SN75LVDS82 suitable? The chip has an LVDS POWER input (PIN 13),
but it's not clear whether you can define +1V8 as the signal level there.
If it doesn't work with the SN75LVDS82, does anyone have an idea which chip I can use,
or is it possible to convert the LVDS level from +1V8 to +3V3 in front of it?
Thanks for your help.