This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD6S300: D+ and D- OVP function for USB type C and max. supported USB2.0 data rate

Part Number: TPD6S300

Tool/software:

Hi, 

we have USB2.0 communication & power on the USB Type-C  connector and we want the OVP feature for DP and DM using the SBU pins on the TPD6S300 where D+ and D- lines from the USB-Type C connector are going to be connected to. 

What is the max. supported data rate for the USB2.0 inerface in that case, 1.5Mbps (LS), 12 Mbps (FS) or 480Mbps (HS)? 

BR