Other Parts Discussed in Thread: TLK110
Hi all,
I have to develop one Ethernet interfaces IEEE802.3 (10BASE-T / 100 BASE-T) and shall be able to detect line short circuiting and line break.
And all Ethernet Interfaces should also support auto line crossing.
For these specification i have to use RJ45 Connector.
Can any one tell me Which RJ45 connector I should use or suggest me the circuitry that i can use for support all the above feature.
Thanks and BR
sanjeev