Part Number: SN65DSI86
Tool/software:
The J722S / AM67x EVK uses the SN65DSI86 DP bridge.
However, we have not yet found a source code to implement the display port.
Is there a roadmap or issues that are open here? The background is that we don't get it running properly on our evaluation board. Currently, it seems that there are no Device Trees supporting Display Port for J722S EVM in TI-Linux-6.12. And I've tried and tested some of the ways
The corresponding sections of the J784S4/J742S2 are to be taken over – this seems to be a bit of a work (depending on the selected one
Resolution / timing I can see activity on the DSI lanes with a Logic Analyzer), but no (valid) signal comes from the monitor
perspective. It would be good to know whether this should work in principle and with which resolutions/timings this was validated.
can you help me, please?