Tool/software:
Hello,
I am currently developing an Ethernet-based application on a Zynq UltraScale+ MPSoC using Vivado 2024.2 and Vitis 2024.2. The system is configured as follows:
-
GEM0 to GEM3 enabled in the Zynq Processing System
-
GT lanes properly assigned
-
Bitstream successfully generated and hardware exported
-
Vitis platform and application created using the exported XSA
The application is based on the lwIP Echo Server template. On boot, the UART console confirms successful application execution and TCP echo server startup. A static IP (192.168.1.10) is assigned to the board.
I am using the TI DP83867ISRGZ Ethernet PHY, interfaced via SGMII. To address PHY negotiation issues, I enabled the sgmii_fixed_link option (set to true) in the lwIP library settings. After this change, the TCP server initializes properly and there are no PHY-related errors reported.
Console Output:
Zynq MP First Stage Boot Loader
Release 2024.2 Apr 30 2025 - 12:44:26
PMU-FW is not running, certain applications may not be supported.
-----lwIP TCP echo server ------
TCP packets sent to port 6001 will be echoed back
Board IP: 192.168.1.10
Netmask : 255.255.255.0
Gateway : 192.168.1.1
TCP echo server started @ port 7
However, I am unable to ping the board from my host PC. Both the board and the host are on the same subnet. TCP connections (e.g., using telnet on port 6001) are functional, but ICMP ping requests do not receive replies.
Could you please advise:
-
Are there any additional PHY register configurations needed for the DP83867ISRGZ when using SGMII fixed link mode?
-
Could any lwIP or MAC configuration be preventing ICMP from working while allowing TCP?
-
Are there known limitations in this setup for ping responses?
Any insights or suggestions would be highly appreciated.
Best regards,
Litesh