Part Number: AM26LS31
Tool/software:


hi team
my customer has been using AM26LS31 and they found that the output of chips with the first silk is 3.8V and the second one is 4.9V . They want to know whether there are any problems?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The die has changed, and now uses CMOS outputs, which can go nearer the supply rails. The outputs are still inside the limits specified by the datasheets (at least 2.5 V for high, or at most 0.5 V for low). This is not a problem.
If this is an ICT, then adjust the high limit (in theory, anything between 2.5 V and 5 V would be OK).