Part Number: DP83869HM
Other Parts Discussed in Thread: DP83869, USB-2-MDIO
Tool/software:
Hello TI team,
I am trying to implement DP83869 in unmanaged copper to fiber mode. I perhaps see copper link, but fiber link is not established, and hence full conversion and communication is broken.
Below some steps and investigation. Please let me know what else should I check, modify and test.
I have checked below things:
1. All power supplies (3.3V, 1.1V, 2.5V) are functional
2. 25 MHz clock is fine - confirmed via checking CLK_OUT (NC on board). Clock shows clean switching with appx 57% duty (slightly longer high than low)
3. Linux OS shows message about Link established and disconnected corresponding to RJ45 connection.
4. LED0 ON, LED2 Intermittently blinking
5. LED1 OFF
6. Fiber Converter module shows no Fiber link.
7. If link loss pass through is enabled - all LEDs will be off after a short blink of LED0, and no link messages on Linux.
8. Captured all register values with USB-2-MDIO tool.
9. Tried to follow steps according to datasheet 7.4.8.6 but that did not restore the link.
Register 0000 is: 3100 Register 0001 is: 7969 Register 0002 is: 2000 Register 0003 is: A0F3 Register 0004 is: 0181 Register 0005 is: C5E1 Register 0006 is: 006D Register 0007 is: 2001 Register 0008 is: 4800 Register 0009 is: 0000 Register 000D is: 401F Register 000E is: F000 Register 000F is: F000 Register 0010 is: 5848 Register 0011 is: 6B02 Register 0012 is: 0000 Register 0013 is: 0000 Register 0014 is: 29C7 Register 0015 is: 0000 Register 0016 is: 0000 Register 0017 is: 0040 Register 0018 is: 6150 Register 0019 is: 4004 Register 001A is: 0002 Register 001E is: 0012 Register 001F is: 0000 Register 0025 is: 0480 Register 002C is: 141F Register 002D is: 0000 Register 002E is: 0221 Register 0031 is: 10B1 Register 0032 is: 0050 Register 0033 is: 0000 Register 0037 is: 0000 Register 0039 is: 0000 Register 003A is: 0000 Register 0043 is: 07A0 Register 004F is: 0200 Register 0055 is: 0000 Register 006E is: 3A0C Register 0071 is: 0000 Register 0072 is: 0000 Register 007B is: 05DC Register 007C is: 007D Register 0086 is: 0077 Register 00C6 is: 0000 Register 00D6 is: 0000 Register 00E9 is: 9F22 Register 00FE is: E721 Register 0134 is: 1000 Register 0135 is: 0000 Register 0136 is: 0000 Register 0137 is: 0000 Register 0138 is: 0000 Register 0139 is: 0000 Register 013A is: 0000 Register 013B is: 0000 Register 013C is: 0000 Register 013D is: 0000 Register 013E is: 0000 Register 013F is: 0000 Register 0140 is: 0000 Register 0141 is: 0000 Register 0142 is: 0000 Register 0143 is: 0000 Register 0144 is: 0000 Register 0145 is: 0000 Register 0146 is: 0000 Register 0147 is: 0000 Register 0148 is: 0000 Register 0149 is: 0000 Register 014A is: 0000 Register 014B is: 0000 Register 014C is: 0000 Register 014D is: 0000 Register 014E is: 0000 Register 014F is: 0000 Register 0150 is: 0000 Register 0151 is: 0000 Register 0152 is: 0000 Register 0153 is: 0000 Register 0154 is: 0000 Register 0155 is: 0000 Register 0156 is: 0000 Register 0157 is: 0000 Register 0158 is: 0000 Register 0159 is: 0000 Register 015A is: 0000 Register 015B is: 0000 Register 015C is: 0000 Register 015D is: 0000 Register 015E is: 0000 Register 015F is: 0000 Register 016F is: 0095 Register 0170 is: 0C0E Register 0172 is: 0000 Register 0180 is: 0752 Register 0181 is: C850 Register 0182 is: 5326 Register 0183 is: A01E Register 0184 is: E976 Register 0185 is: 19CF Register 0190 is: 0000 Register 0191 is: 0000 Register 0192 is: 0000 Register 0193 is: 0000 Register 0194 is: 0000 Register 0195 is: 0000 Register 0196 is: 0000 Register 0197 is: 0000 Register 0198 is: 0000 Register 0199 is: 0000 Register 01A4 is: 0000 Register 01A5 is: 0000 Register 01A6 is: 0000 Register 01A8 is: 0000 Register 01A9 is: 0000 Register 01DF is: 0005 Register 01E0 is: 417A Register 01EC is: 1FF5 Register 0C00 is: 2100 Register 0C01 is: 6149 Register 0C02 is: 2000 Register 0C03 is: A0F3 Register 0C04 is: 0020 Register 0C05 is: 0000 Register 0C06 is: 0000 Register 0C07 is: 2001 Register 0C08 is: 0000 Register 0C10 is: 3148 Register 0C18 is: 01FF Register 0C19 is: 0000