Part Number: DP83561-SP
Tool/software:
The IBIS model provided for the DP83561-SP has all of the TD pins marked as input only despite these pins being I/O.
Is there a version of the IBIS model that provides the TD pin as outputs?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83561-SP
Tool/software:
The IBIS model provided for the DP83561-SP has all of the TD pins marked as input only despite these pins being I/O.
Is there a version of the IBIS model that provides the TD pin as outputs?
Hi Ryan,
By 'TD' Pins are you referring to the MDI-side TD_P_A/B/... pins or the MAC-side TX_D0/1/... pins?

Best,
Shane
Hi Shane,
I was referring to the MDI-side TD_P_A/B/etc pins.
My goal was to simulate between these pins and the magnetics on my design. I assume the response is the same as the other E2E then?
Hi Ryan,
Yes you are correct. Unfortunately we don't have an IBIS model that tracks the MDI-side pins.
Best,
Shane