Part Number: SN65HVD72
Tool/software:
Hi,
Our current design uses ST1480ABDR IC from ST. We have found that, few PCBs failed to work.
This is easy to reproduce at 70 degC. Problem can be seen within 2 hours After some research I found that, in some applications the fail safe bias resistors are require at A and B.
I tested with external fail safe resistors with ST part ST1480ABDR and the problem was resolved.
Now , we have thousands of PCBs made for our production. so I decided to use SN65HVD72DR TI part with internal bias resistors.
When I tested at 70 deg with two different PCBs, One PCB worked well without any issues. second PCBs failed after 8 hours.
Could you please help me to check this issue? Does this IC also need external Bias resistors?
If you can provide an email address, I will share the schematics. this issue is urgent as our production is on hold now.
Thanks
Parvin