Part Number: TLK2711-SP
Tool/software:
Hi,
We use two TLK2711AIRCP components (now obsolete) in the circuit. Recently, some cards have shown a current consumption 30mA higher than expected, when the TLK2711 components are placed in power-down mode. We checked with a thermal camera and saw that the temperature of one of the components was 1.5 degrees higher than similar cards. Functionally, the component worked properly.
After replacing the component, the current consumption decreased.
Does the high current consumption in power-down mode indicate a problem with the component?
Thank you