Part Number: DS90UB935-Q1
Tool/software:
Hi Support team,
I'm member of PoC support team of TDK.
Our customer will use DS90UB935-Q1 as serializer in synchronous mode, and it will be connected to de-serializer for FPD-Link III / IV.
- In this case, minimum back channel rate is 25Mbps? 50Mbps?
- If the back channel is 25 Mbps (or 50Mbp), should the frequency range for the PCB S-parameter Limit line be referenced from 12.5 MHz (or 25MHz)?
- If the PCB S-parameter limit line is satisfied, is it acceptable for the coil's inductance value to be less than 10 µH?
Best regards,
Takatoshi Ike