Part Number: DP83867ERGZ-R-EVM
Other Parts Discussed in Thread: DP83867ERGZ-S-EVM
Tool/software:
Hello,
I would like to connect two computers to each other via a network interface card. However, between the two ethernet cables, I'd like to use SGMII for a project. I have (2) DP83867ERGZ-R-EVM boards. What is the minimum need to do to connect the boards? Is there any configuration needed on the computer? Do the RJ45 cables need to be special? When making reference to signals, please also reference the connector and pin number. For example, I can't find any documentation that tells me what pin TX_D0 is connected to on J3.