This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCA9306: PCA9306, Is it okay to use Vref1 2.8V and Vref2 3.3V for PCA9306?

Part Number: PCA9306

Tool/software:

Hi, 

I saw the datasheet that has recommended SCH with 1.8v as Vref1, 3.3v as Vref2.. 

also found that 

VREF2 must be between VREF1 + 0.6 V to 5.5 V in datasheet P5, 6.3 Recommended Operating Conditions

I was wondering the following may not be okay. 

2.8v as Vref1, and 3.3v as Vref2?

Am I right?

Thanks

JIE