Part Number: TS3USB3000
Tool/software:
HI Sir
Did the TS3USB3000 can input the bipolor waveform?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
The TS3USB3000 has analog voltage io rating of 0V to 3.6V 
However because this is a usb 2 switch and you are likely passing USB 2 signals which means the actual voltages signals you are passing through the device (D- and D+) just have opposite polarity.
This is differential signaling and it looks like this

So two +500mv differential pair signals is fine to pass through this device.
Please let me know if I am misunderstanding and we can discuss more.
Regards,
Kameron