We recently purchased a product that uses the 26LS33AC chip as an encoder counter. The manufacturer suggests leaving pins 1, 6, 7, 9, and 10 disconnected if we are only using a single digital input. What does the manufacturer recommend be done with these connections when not in use?
Our end result is that the pin 1 has floated to a higher voltage and we are seeing only 40 kohms to ground but are seeing 100 kohms for the rest of the pins, as the document suggests we should. Is there something that we can do to prevent this from happening in the future?
We were able to fix this problem by adding a 4.3kohm resistor to ground and the voltage on pin 1 seems to be what it should.
Thank you very much