Tool/software:
Hi,
I’m designing a board using the TUSB8041 where the upstream port is directly connected to a Raspberry Pi CM5. In this setup, there is no physical USB connector on the upstream port, and therefore, no standard VBUS source.
The TUSB8041 is powered entirely from a 3.3V rail, which is always present during normal operation. I would like to simulate the USB_VBUS detection using a voltage divider from this same 3.3V rail, using 150 kΩ and 27 kΩ resistors, which results in approximately 0.51V at the USB_VBUS pin.
Would this configuration be acceptable?
-
Can USB_VBUS safely be derived from the same 3.3V rail that powers the hub itself?
-
Are there any concerns with using this divider setup in a production system?
Thanks in advance for your support.
Best regards,