Part Number: DS280DF810
Tool/software:
Hi team,
Customer is using DS280DF810ABVR, set receiver adapt mode 2.When I write Reg_0x0a to reset CDR channel,sometimes the CTLE value adapts to 0x00, sometimes the CTLE value adapts to 0x04. The value of VEO will vary significantly depending on the value of CTLE. A good CTLE value ,VEO can reach up to 0x60. while a poor CTLE value ,VEO can only reach 0x3c. Therefore, I want to limit the value of VEO to be greater than 0x40 (200mV) before CDR stops adapting .I found Reg_0x6a, but the maximum VEO value it can set is 15 * 4 * 3.125mV=187.5mV, which does not meet my requirements .Is there any other way to limit the value of VEO to be greater than 0x40 (200mV) or 0x50 (250mV)?
Thanks.
Regards,
Wesley