Part Number: TMUXHS4446
Other Parts Discussed in Thread: TMUXHS4612, HD3SS3220
Tool/software:
Hi,
-
Do we have a similar mux that supports DisplayPort 2.1 UHBR20 (20 Gbps)?
-
In this mux, can I route USB SuperSpeed (USB SS) signals through the DP input pins, since those I/Os are listed as "I/O" in datasheet?
-
Is there an external GPIO(Select line) pin available for selecting between the USB SS and DP paths, or is this selection managed solely through I²C control?
-
Is there an external pin to indicate USB-C cable orientation (flip detection), or is this also handled via I²C?