Part Number: P82B96
Other Parts Discussed in Thread: INA260, INA228, , TIDA-01608, ISO7842, ISOW7842
Tool/software:
I've used this part (P82B96) as part of the TIDA-01608 reference design but replaced the current sensor with a INA228. The communications does not work. I've scoped the communications and found that the output of the P82B96 only gives a 0.8V low logic level which is higher than the INA228 spec in the datasheet. The Datasheet lists 0.4V or less. The original INA260 would work to 0.3*VS which I missed. I've attached the scope output and the schematic in pdf and screen capture form. The purple on the scope is the isolated ground of the INA228 and P82B96. The yellow is SCL and green/blue is SDA. The INA228 is not acknowledging receipt of the packet. I've verified the address etc. I assume the reference design worked with the higher VIL of the INA260 but the question is how can I make this work without a board spin?