Part Number: SN75DPHY440SS
Tool/software:
Hi, TI expert
The customer used SN75DPHY440SS while using MIPI output camera in the existing project.
However, during the development of a new project, the camera was changed to omnivision analog type instead of MIPI output camera, and the transmission distance is long, causing problems with jitter and image quality.
Accordingly, I am looking for another IC because I don't think I can apply SN75DPHY440SS used in the existing MIPI camera.
The actual signal waveform is as shown in the picture below.
(※ Image output (VOUT_: Analog signal and SPI signal are combined))

Can you recommend an IC that can be used in the image output, such as RETIMER, Equalizer, Redriver, and buffer?
Please check. Thank you.