Other Parts Discussed in Thread: TLIN2021-Q1
Tool/software:
Dear team
our customer's Automotive HVAC motor team recently encountered a problem about the testing ISO21780 (test-12) Ground Loss
Once the 48V motor disconnects from the ground trace, the motor MCU based driver’s integrated LIN transceiver injects the voltage, causing the LINBus ramping to 29V.
According to ISO21780 test 12, the voltage of the LINbus should not exceed 16V.
our customer right now wants to know whether implementing the discrete (external) LIN transceiver, Like our TLIN2021-Q1, can help it pass the ISO21780 test 12.
If implement only TLIN2021-Q1 cannot solve the problem, please suggest adding other device or circuitry. Sincerely thanks!!!
Best regards,
Hank Lin