Part Number: DS90UB953-Q1
Tool/software:
dear ti team
I just saw the comment "954, the latency is dominated by the line buffer in the 954. Other latency from 953 serialization and prop delay through the cable are small compared to the 954 line buffer time.
The 954 buffers up to 2 lines from each RX port, so the latency can be roughly equated as 2x the line time.
Ex. For 1280x800 @ 60Hz, the video line time is ~20.1us:
So total buffer time would be ~40.2us which roughly equals the total latency through the 953/954 chain. "
I want confirm that when the whole image has been sent, it should take 800/2 times 40.2us = 400*40.2us= 16080us= 1.6ms