This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-AM261: Phy on fixed speed need seconds to establish a link

Part Number: LP-AM261

Tool/software:

Dear Sir or Madam,

on the evaluation board AM261x,AM263P we have problems with the phy. If the phy is set to a fixed speed: 10 Mbit/s half duplex; 10 Mbit/s full duplex; 100 Mbit/s half duplex or 100 Mbit/s full duplex, it needs sometimes seconds to establish a link. We guess the phy itself don’t have a problem - but the phy driver.

Software that is used, INDUSTRIAL-COMMUNICATIONS-SDK-AM263PX/AM261x — Industrial Communications SDK with EtherNet/IP.

Scenario:

If you plugin in and pull out the ethernet cable, several times directly one after the other, the phy will need seconds to establish a link.

For some applications it is necessary to send the first ethernet message under 500ms - reliable.

Could you please verify if the failure is in the phy driver or in the phy itself?

If the phy itself has the problem could you please provide a phy that match the requirement?

Best regards