Part Number: DP83869HM
Other Parts Discussed in Thread: DP83869
Tool/software:
Hi
We have designed a circuit which includes a DP83869 operating in media converter mode.
The SFP is an FS.com generic SFP module
We are configuring it using an external microcontroller communicating over the MDIO interface
When the optical side is connected to a commercial media converter, the link comes up OK and we can send data from one PC to another through the link.
When we connect two of our circuits together, the link fails to come up 99 times out of 100.
Our feeling is that this is an autonegotiation issue but we'd appreciate any advice or assistance to help us resolve the issue.
We have run through the troubleshooting guide and the schematic review and didn't see any major errors (except the signal detect line, which we failed to pull high,)
We do have a microcontroller connected to the MDIO interface and use this for initial setup.Single-Board-WOLF-Media_Converter.pdf