Hi,
I am looking for a solution for HDMI Splitter which is HDCP compliant. Please help me in finding the necessary reference design or IC.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am looking for a solution for HDMI Splitter which is HDCP compliant. Please help me in finding the necessary reference design or IC.
Thanks for your help. But i need a Splitter not a switch. I got an ic MAX3845 which is 2:4 fan out switch and cable driver but the problem is that it can split the input to all the outputs if the input is not HDCP compliant. I need a splitter ic which can split the signal which is HDCP compliant. please suggest me a solution.
Thanks ,
harsha vardhan
The TMDS442 can be configured as a fan out (just connect both outputs to the same input), but you will not be able to transmit HDCP encoded data to both sinks simultaneously. To do this, the fanout must have a full HDCP engine on each output to encrypt signals to each sink.