Part Number: TSD05
Other Parts Discussed in Thread: , TVS0500
Tool/software:
Hi,
I have a question about how to use and select a TVS.
Target parts: TSD05, TSD05C
Things to check
①. Is it okay to use it for the following purposes?
- Between the signal and GND of a small signal line (5V analog input)
- Lightning surge protection for a subsequent IC (maximum rated DC7V)
②. Is it possible to protect the subsequent IC against the following surges by using lightning surge protection for a signal line?
- Applied voltage: ±2.0kV, 1.2/50μS
- Discharge interval: 60s
- Applied location: Signal line - GND (TVS mounting location)
③. Is it possible to use two TSD05 (unidirectional) in series in the opposite direction? (Is this a common usage?)
If it is possible, I think the clamp voltage will increase by the forward voltage, is this correct?
Will the internal capacitance be halved?
*For reference, the Toshiba DF2B7PCT,L3F currently under evaluation was broken by a surge, and then the downstream IC was broken.
Diodes D5V0S1B2LP-7B passed the surge test, but was affected by leakage current and capacitance, and the product performance was
not satisfactory. (The product performance is designed with severe leakage current and capacitance.)
④. Sorry, but could you please introduce any other parts you could suggest?
The specifications are roughly as follows.
<Product performance test conditions>
-Leakage current (IR): 1μA or less
-Internal capacitance (Ct): 50pF or less
-Operating voltage (VRWM): 5.5V or more
<Surge test conditions>
-Signal line surge resistance: ±2.0kV (lightning surge test: IEC61000-4-5 compliant, 1.2/50μs combination waveform)
-Limit (clamp) voltage (VC): 11Vmax or less
-Peak pulse current (Ipp): 40Amax or more or peak pulse power (PPPM): 400W or more
Best regards,
Hiroshi