This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD1780: Communication error and abnormal response from the Slave devices

Part Number: SN65HVD1780

Tool/software:

Greetings,

I am using SN65HVD1780 IC for RS485 communication between my master and slave devices. Cable length is less than 50 meters and baudrate is 9600. I have used 120 Ohm termination resistor at the both end of the network. 

Issue is that when I use USB to RS485 converter  and read every single node by converter it works perfectly; but when I connect slaves with my master device few random slave devices does not respond to query. 

I am using daisy loop network and 4.7K resistor for the pull-up (A+) and pull-down(B-).