Part Number: AM26LS32AC
Other Parts Discussed in Thread: AM26C32,
Tool/software:
We have been producing boards with AM26LS32ACD for many years and during testing we check the current absorption on 5V. Normally we have an absorption of about 40mA per chip.
In the latest production, however, the absorption has become practically zero.
For this reason we have studied the issue in depth by creating two small wired boards where we have placed a previous chip (which we indicate with A) that consumes 40mA and a recently purchased one (which we indicate with B) that consumes 0mA.
In the boards created for the test we have connected only the +5V power supply on pins 16 and 4 while we connected the GND to pins 8 and 12. In this way the integrated circuit is powered and enabled (G signals activated).
Device A absorbs 40mA while device B absorbs almost zero mA.
Device A has the Texas logo printed on it and was purchased on DigiKey while device B does not have the Texas logo but the "TI" text and was purchased on a reel directly from the Texas Instruments e-store.
The printing on the device is identical except for the logo (symbol and text) and the supplier (DigiKey and Texas).
The datasheet indicates a consumption of about 50mA but we do not explain this difference. Such a high difference should be documented and the chip should have a different code.
Finally, both boards produced work with both devices apart from the different consumption.
But, since there are three devices per board, the total consumption is considerable and this is a problem.
Thanks