Tool/software:
Dear TI experts,
My customer is looking for the device which can protect surge situation.
My customer said that it should be protected 2000V based on IEC 61000-4-5.
But in the datasheet it says ;
Peak pulse power (8/20us)(max) = 28000W
IEC 61000-4-5 = 60A
Vrwm = 24V
Can it protect 2000V? or just can protect up to 24V?
Could you recommend protection IC which my customer is looking for?
Best regards,
Chase