Part Number: THVD4411
Tool/software:
Hi there,
I want to (have to) operate the THVD4411 with only 3 GPIO pins of our microcontroller. Shoul it work like in the following schematics?
- GPIO-1 is assigned to DIR
- GPIO-2 to Mode-0
- GPIO-3 to Mode-1, TERM_TX and TERM_RX
- SHDN = always VIO (Device always enabled)
I want to use the Mode-1 signal for terminal resistors as well since this signal must always high if any RS485 mode is chosen.
- Do you see any problem if the terminal resistor on the R3/R4 is also enabled on the RS485 half duplex mode?
- SHDN = always VIO (Device always enabled). Should it be OK if the device is always enabled on the RS232 mode.
- Are the function names OK on the common connector X13?
Thank you very much!
Best regards,
Aziz