Part Number: DP83TC817S-Q1
Other Parts Discussed in Thread: DP83TC811
Tool/software:
Dear Suppor,
We are currently trying to analyze a problem with the DP83TC817-Q1. We are developing boundary scan tests.
A loopback has probably already been implemented here.
We are currently trying a static loopback test via the MII loopback function of this module.
We set this loopback mode via the MDIO interface register 0x00 to the value 0x6100.
Then we try to drive static levels at TX0 and TX1 and then try to measure these levels back at RX0 and RX1.
The TX_EN signal is driven high during this process.
But unfortunately we cannot measure any change in the RX signals. We can measure and describe the register values. That all seems to work.
Now the question is whether this can work statically and what other conditions may have to be met to realize such a static loopback test. (Without using functional protocols)
It would be nice if you could support us here.
Thanks Jan Balzer