Tool/software:
Here is the table set the 963 and 960 serdes.
Right now frame received by 960. but the image line size is not correct. Can you help with the problem?
the sensor IMX623 output setting is 1920*1536 raw12 30fps.
right read the 0x73-0x76 show that the 0x06 0x14(1539) 0x0b 0x58(2904).
root@am62axx-evm:/opt/edgeai-gst-apps# i2ctransfer -y 2 w1@0x30 0x73 r4
0x06 0x14 0x0b 0x58
root@am62axx-evm:/opt/edgeai-gst-apps# i2ctransfer -y 2 w1@0x30 0x90 r2
0x07 0x3f
root@am62axx-evm:/opt/edgeai-gst-apps# i2ctransfer -y 2 w1@0x30 0x90 r2
0x00 0x5d
root@am62axx-evm:/opt/edgeai-gst-apps# i2ctransfer -y 2 w1@0x30 0x5c r2
0x30 0x34
root@am62axx-evm:/opt/edgeai-gst-apps# i2ctransfer -y 2 w1@0x30 0x57 r2
0x00 0x5e
root@am62axx-evm:/opt/edgeai-gst-apps# i2ctransfer -y 2 w1@0x30 0x55 r4
0x00 0x00 0x00 0x5e
root@am62axx-evm:/opt/edgeai-gst-apps# i2ctransfer -y 2 w1@0x30 0x7a r2
0x0d 0xff
root@am62axx-evm:/opt/edgeai-gst-apps# i2ctransfer -y 2 w1@0x30 0x4d r2
0x13 0x45
root@am62axx-evm:/opt/edgeai-gst-apps# i2ctransfer -y 2 w1@0x30 0x35 r1
0x01
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps# i2ctransfer -y 2 w1@0x18 0x52 r1
0x45
root@am62axx-evm:/opt/edgeai-gst-apps# i2ctransfer -y 2 w1@0x18 0x57 r1
0x00
root@am62axx-evm:/opt/edgeai-gst-apps# i2ctransfer -y 2 w1@0x18 0x5c r2
0x02 0x00