This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVDS100: About the input eyemask of SN65LVDS100

Part Number: SN65LVDS100


Tool/software:

Hi

The output of CML Device is connected to the input of SN65LVDS100.
I want to test whether the output of CML Device meets the AC input characteristics of SN65LVDS100.
We are currently producing an eye diagram mask that meets the input AC characteristics of SN65LVDS100.
I saw the INPUT CHARACTERISTICS related to the voltage of SN65LVDS100 in the datasheet,
However, I can not find the AC INPUT CHARACTERISTICS related to SN65LVDS100 correctly,
Could you help confirm the time of point A and point B in the picture?


Can you please provide the evidence in the data manual for determining the time of point A and point B?
The midpoint in the figure is 0 nanoseconds.

If there are any errors in the voltage, please help correct them.

Thanks and Best Regards

Chunli Liang