Tool/software:
Hi
The output of LVDS Device is connected to the input of SN65CML100.
I want to test whether the output of LVDS Device meets the AC input characteristics of SN65CML100.
We are currently producing an eye diagram mask that meets the input AC characteristics of SN65CML100.
I saw the INPUT CHARACTERISTICS related to the voltage of SN65CML100 in the datasheet,
However, I can not find the AC INPUT CHARACTERISTICS related to SN65CML100 correctly,
Could you help confirm the time of point A and point B in the picture?

Can you please provide the evidence in the data manual for determining the time of point A and point B?
The midpoint in the figure is 0 nanoseconds.
If there are any errors in the voltage, please help correct them.
Thanks and Best Regards
Chunli Liang