Part Number: TDP1204
Tool/software:
Dear TI's expert,
When I set the TDP1204 to pin-strap mode, does the TXPRE setting affect the pre-emphasis of the HDMI 2.1 eye diagram test?
I have this question because I don't quite understand Table 8-16—what determines the TXFFE adjustment from 0 to 3?
The picture as below shows the HDMI 2.1 eye diagram test for Lane 0. Regardless of my TXPRE settings, the HDMI 2.1 eye diagram's result didn't change. Even adjusting the EQ settings makes the eye diagram worse.
I would like to confirm whether there is an error in my setting.
Below is my hardware setup:
CFG0 = 0
AC_EN = 0
MODE = 0
LINEAR_EN = 0
CTLEMAP_SEL = 0
EQ0/EQ1 = 00
TXPRE = 1
TXSWG = 0
Thank you for any help you can provide.