Part Number: SN65LVDS391
Other Parts Discussed in Thread: TXU0104
Tool/software:
Hello Team,
We have a product with SN65LVDS391PW and SN65LVDS32PWR to convert LVDS to CMOS and vice versa.
These driver/receiver are connected to a 3.3V MCU. The intention is to convert the single ended SPI signals from the MCU to convert to LVDS signal.
On the slave side of the SPI, we are using the same drivers/receivers to convert from LVDS to single ended signal.

The SPI is working in 10MHz frequency.
In our new system, our sensor is replaced with a 1.8V sensor.
1). Can anyone please suggest a 1.8V to 3.3V level converter that we can use here that will not effect the speed/ functionality of the system?.